Python Script Execution

When developing Python scripts for ADS (or DDS*), it is important to consider the execution context the script runs in, as the set of available functionality differs depending on whether or not the script executes within the context of the application.

When executing scripts from within the ADS application, whether from the Python console, an addon, or menu action, etc., application level functionality is available, you can display a message box or access a window, for example. Scripts executing outside the application context do not have access to ADS application functionality, such as user interface and interprocess communication. This includes, but is not limited to, the keysight.ads.de.app package and AEL application functions that interact with the user interface or access the simulator in some manner. Simulation in automation mode can make use of the keysight.edatoolbox package, which is beyond the scope of this document.

To determine if the executing context is the ADS application, the script can check keysight.ads.de.is_pde_app().

*Note: DDS is the Data Display application, which is a separate application that can be launched from the command line or from within ADS. Both ADS and DDS have their own embedded Python interpreter and are separate execution contexts.

Automation

‘Automation’ is a term used to describe when the execution context of an extension module is not the owning application. Importing the keysight.ads.de or keysight.ads.dds packages directly into a Python process is considered ADS or DDS automation, respectively. Additionally, importing the keysight.ads.dds package from within the ADS application is considered DDS automation, just as importing keysight.ads.de from within the DDS application is considered ADS automation.

When running in an automation mode (ADS, DDS, or both), scripts are not able to access the associated application’s user interface. For example, when running scripts inside ADS, the DDS user interface APIs are not available, and vice versa. Examples of UI functionality include, but are not limited to: windows, message boxes, palettes, menus, and toolbars.

To determine if a particular execution context is automation, the script can check the return value of the appropriate is_app function, for ADS, this is keysight.ads.de.is_pde_app(), and for DDS, this is keysight.ads.dds.is_dds_app().

Note: The keysight.ads.de.running_automation() and keysight.ads.dds.running_automation() functions are misnamed and those names will be deprecated in a future release. Both functions mean the same thing, that the script is not executing in either the ADS or DDS application context, but a Python application context.

The following examples demonstrate the different results of the is_pde_app, is_dds_app, and running_automation functions when executed from different contexts:

From within the ADS application:

../../_images/ADS_app_automation_modes.png

From within the DDS application:

../../_images/DDS_app_automation_modes.png

From the command line:

../../_images/Automation_mode.png
On this page