Transaction
Classes
- class keysight.ads.de.db.Transaction
Operations performed between when the Transaction is created and when it is committed may be undone.
This provides the ability to group multiple operations together and undo them with a call to rollback.
- commit() None
- is_empty() bool
- rollback() None
- property state: TransactionState
Enumerated Types
- class keysight.ads.de.db.TransactionState
An enumeration specifying the state of a design transaction.
- IN_PROGRESS = <TransactionState.IN_PROGRESS: 0>
The transaction is in progress.
- COMMITTED = <TransactionState.COMMITTED: 1>
The transaction has been committed.
- ROLLED_BACK = <TransactionState.ROLLED_BACK: 2>
The transaction has been rolled back.