Examples
The source code for the examples referenced by these help pages can be found in $HPEESOF_DIR/de/python
Contents:
- Calling Between AEL and Python
- Create Layout
- Create Schematic
- Create Workspace
- Create, Simulate, and Plot
- Interoperable Component Parameters
- Component Parameters
- Creating an Item Definition
- Model Definition Properties
- Adding Instances to a Design
- Properties
- Creating Custom Menus Using an Addon
- Padstacks and Vias
- Nested Technology
- Rules
- Placing Text
- Paths, Traces, and Polygons
- PySide2
- Traversing Hierarchy
- Working with VAR
- XML RPC
- GDSII Import and Export