Nested Technology
Classes
- class keysight.ads.de.tech.nested.LayerMap
LayerMap is a mapping of selected layers in a nested library to layers on the parent library.
The nested library is assumed to have a different technology than the parent library. One or more layers from the nested library can be mapped to equivalent layers in the parent library.
- property name: str
The name of the layer mapping. Used on nested substrate items.
- property nested_library_name: str
- property layer_map_library_name: str
The name of the layer mapped library. Usually the parent library name.
- property is_above: bool
Are the nested layers above the layers on the parent.
- property is_flipped: bool
Are the nested layers flipped.
- property nested_mapped_layers: ListRefAbc[str]
Return the collection of nested mapped layer names in this LayerMap.
These are the source layers from the nested library that are mapped.
- property parent_mapped_layers: ListRefAbc[str]
Return the collection of parent mapped layer names in this LayerMap.
These are the mapped layers in the parent library.
- map_nested_layer(nested_layer_name: str) None
Add a mapping between the nested layer and a layer in the parent.
Note: This does not add the layers to the parent technology.
- unmap_nested_layer(nested_layer_name: str) None
Remove the mapping between for the nested layer.